SBVS303B March 2017 – February 2018 TPS3890-Q1
PRODUCTION DATA.
A typical application for the TPS389018-Q1 is shown in Figure 25. The TPS389018-Q1 can be used to monitor the 1.8-V VDD rail required by the TI Delfino™ microprocessor family. The open-drain RESET output of the TPS389018-Q1 is connected to the XRS input of the microprocessor. A reset event is initiated when the VDD voltage is less than VITN or when MR is driven low by an external source.