SLUSBO6C JANUARY 2014 – October 2018 TPS40425
PRODUCTION DATA.
| Format | Unsigned binary integer | ||||
| Description | The SEQUENCE_TON_TOFF_DELAY command is used to set the delay for turning on the device and the delay for turning off the device as a ratio of TON_RISE.
This is a paged register. In order to access this register for channel 1 of the TPS40425 device, PAGE must be set to 0. In order to access this register for channel 2 of TPS40425 controller, PAGE must be set to 1. For simultaneous access of channels 1 and 2, PAGE command must be set to 11. If the channel is configured as a SLAVE, this command can not be accessed for that channel. Any writes to the SLAVE channel for this command are ignored. In such a case, internally the TON_DELAY is set to the minimum value of 50 µs and TOFF_DELAY is set to zero (overriding any contents of EEPROM). An attempt to read and write the SLAVE channel command results in a NACK’d command and the reporting of an IVC fault and triggering of SMB_ALERT. |
||||
| Default | 000X 000X (binary)
The default power-up state can be changed using the STORE_USER commands. |
||||
| PAGE0, PAGE1 | |||||||
| r/wE | r/wE | r/wE | r | r/wE | r/wE | r/wE | r |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| TON_DEL<2:0> | X | TOFF_DEL<2:0> | X | ||||
| Bits | Field Name | Description |
|---|---|---|
| 7:5 | TON_DEL<2:0> | (Format: binary)
Default: 000b TON_DELAY = TON_RISE × TON_DEL<2:0> This parameter controls the delay from when ON = 1 until the soft-start sequence begins. The default value is 0 ms. (Start the VOUT ramp without delay) |
| 4 | X | X indicates writes are ignored and reads are 0 |
| 3:1 | TOFF_DEL<2:0> | (Format: binary)
Default: 000b TOFF_DELAY = TON_RISE × TOFF_DEL<2:0> This parameter controls the delay from when ON = 0 until the output is disabled. The default value is 0 ms. (Shut off the output without delay) |
| 0 | X | X indicates writes are ignored and reads are 0 |
| TON_DEL<2:0>
TOFF_DEL<2:0> |
DELAY TIME RATIO
(MULTIPLE OF TON_RISE) |
|---|---|
| 000 | 0(1) |
| 001 | 1 |
| 010 | 2 |
| 011 | 3 |
| 100 | 4 |
| 101 | 5 |
| 110 | 6 |
| 111 | 7 |
.
NOTE
If the device turns off due to a turn-off delay time, any attempt to turn on the device before the turn-off delay time expires should be avoided. The device is available to be turned on only after the turn-off delay time expires and the device has been turned off,