SLUSBO6C JANUARY 2014 – October 2018 TPS40425
PRODUCTION DATA.
PIN NAME | DUAL OUTPUT | 2-PHASE |
---|---|---|
RT | Connecting a resistor from this pin to AGND | Connecting a resistor from this pin to AGND |
SYNC | Floating or connect to external clock | Floating or connect to external clock |
PHSET | Floating | Floating |
FB1 | Inverting input to the error amplifier 1 | Inverting input to the error amplifier 1 |
FB2 | Inverting input to the error amplifier 2 | Connect to BP5 |
COMP1 | Output of the error amplifier 1 | Output of the error amplifier 1, connect to COMP bus |
COMP2 | Output of the error amplifier 2 | Connect to COMP bus |
ISH1 | Floating | Connect to ISH bus |
ISH2 | Floating | Connect to ISH bus |
FLT1 | Fault inductor of CH1 | Connect to FLT bus |
FLT2 | Fault inductor of CH2 | Connect to FLT bus |
PG1 | Power good indicator for CH1 output voltage, connect to BP5 via a pull-up resistor | Power good indicator for 2-phase output voltage, connect to BP5 via a pull-up resistor |
PG2 | Power good indicator for CH2 output voltage, connect to BP5 via a pull-up resistor | Floating or connect to GND |
VSENS1 | Positive pin of Voltage Sense Signal for CH1 | Positive pin of Voltage Sense Signal for 2-phase output |
GSENS1 | Negative pin of Voltage Sense Signal for CH1 | Negative pin of Voltage Sense Signal for 2-phase output |
VSENS2 | Positive pin of Voltage Sense Signal for CH2 | Connect to GND is recommended. Connect to the output voltage is also allowed. |
GSENS2 | Negative pin of Voltage Sense Signal for CH2 | Connect to GND |
CNTL1 | Logic level input which starts or stops CH1 | Logic level input which starts or stops both channels. |
CNTL2 | Logic level input which starts or stops CH2 | Floating |
DIFFO1 | Remote Sense Amplifier Output for CH1 | Remote Sense Amplifier Output for 2-phase |
AVSDATA | AVS data(1) | AVS data for 2-phase(1) |
AVSCLK | AVS CLOCK(1) | AVS CLOCK for 2-phase(1) |
DEVICE | PIN NAME | 3-PHASE | 4-PHASE |
---|---|---|---|
IC1
(Master) |
RT | Connecting a resistor from this pin to AGND, use the same RT resistor value for IC1 and IC2 | Connecting a resistor from this pin to AGND, use the same RT resistor value for IC1 and IC2 |
SYNC | Connect to SYNC bus | Connect to SYNC bus | |
PHSET | Connect to PHSET bus | Connect to PHSET bus | |
FB1 | Inverting input to the error amplifier 1 of IC1 | Inverting input to the error amplifier 1 of IC1 | |
FB2 | Connect to BP5 of IC1 | Connect to BP5 of IC1 | |
COMP1 | Output of the error amplifier 1of IC1, connect to COMP bus | Output of the error amplifier 1 OF IC1, Connect to COMP bus | |
COMP2 | Connect to COMP bus | Connect to COMP bus | |
ISH1 | Connect to ISH bus | Connect to ISH bus | |
ISH2 | Connect to ISH bus | Connect to ISH bus | |
FLT1 | Connect to FLT bus | Connect to FLT bus | |
FLT2 | Connect to FLT bus | Connect to FLT bus | |
PG1 | Power good indicator for 3-phase output voltage, connect to BP5 via a pull-up resistor | Power good indicator for 4-phase output voltage, connect to BP5 via a pull-up resistor | |
PG2 | Floating or connect to GND | Floating or connect to GND | |
VSENS1 | Positive pin of Voltage Sense Signal for 3-phase output | Positive pin of Voltage Sense Signal for 4-phase output | |
GSENS1 | Negative pin of Voltage Sense Signal for 3-phase output | Negative pin of Voltage Sense Signal for 4-phase output | |
VSENS2 | Connect to GND is recommended. Connect to the output voltage is also allowed. | Connect to GND is recommended. Connect to the output voltage is also allowed. | |
GSENS2 | Connect to GND | Connect to GND | |
CNTL1 | Logic level input which starts or stops 3-phase | Logic level input which starts or stops 4-phase | |
CNTL2 | Floating | Floating | |
DIFFO1 | Remote Sense Amplifier Output for 3-phase | Remote Sense Amplifier Output for 4-phase | |
AVSDATA | AVS data for 3-phase(1) | AVS data for 4-phase(1) | |
AVSCLK | AVS CLOCK for 3-phase(1) | AVS CLOCK for 4-phase(1) | |
IC2
(Slave) |
RT | Connecting a resistor from this pin to AGND, use the same RT resistor value for IC1 and IC2 | Connecting a resistor from this pin to AGND, use the same RT resistor value for IC1 and IC2 |
SYNC | Connect to SYNC bus | Connect to SYNC bus | |
PHSET | Connect to PHSET bus | Connect to PHSET bus | |
FB1 | Connect to BP5 of IC2 | Connect to BP5 of IC2 | |
FB2 | Inverting input to the error amplifier 2 of IC2 | Connect to BP5 of IC2 | |
COMP1 | Connect to COMP bus | Connect to COMP bus | |
COMP2 | Output of the error amplifier 2 of IC2 | Connect to COMP bus | |
ISH1 | Connect to ISH bus | Connect to ISH bus | |
ISH2 | Floating | Connect to ISH bus | |
FLT1 | Connect to FLT bus | Connect to FLT bus | |
FLT2 | Fault indicator for CH2 of IC2 | Connect to FLT bus | |
PG1 | Floating or connect to GND | Floating or connect to GND | |
PG2 | Power good indicator for CH2 output voltage of IC2, connect to BP5 via a pull-up resistor | Floating or connect to GND | |
VSENS1 | Connect to GND is recommended. Connection to the output voltage is also allowed. | Connect to GND is recommended. Connection to the output voltage is also allowed. | |
GSENS1 | Connect to GND | Connect to GND | |
VSENS2 | Positive pin of Voltage Sense Signal for CH2 of IC2 | Connect to GND is recommended. Connect to the output voltage is also allowed. | |
GSENS2 | Negative pin of Voltage Sense Signal for CH2 of IC2 | Connect to GND | |
CNTL1 | Connect to CNTL1 of IC1 | Connect to CNTL1 of IC1 | |
CNTL2 | Logic level input which starts or stops CH2 of IC2 | Floating | |
DIFFO1 | Floating | Floating | |
AVSDATA | Can be used for CH2 of IC2.(1) | See (1) | |
AVSCLK | Can be used for CH2 of IC2.(1) | See (1) |