SLUSBO6C JANUARY 2014 – October 2018 TPS40425
PRODUCTION DATA.
The VIN_OFF command sets the value of the input voltage at which the unit should stop power conversion.
Values written within the supported VIN range are mapped to the nearest supported increment.
The supported VIN_ON values are:
4 (default) | 4.25 | 4.5 | 4.75 | 5 | 5.25 | 5.5 |
5.75 | 6 | 6.25 | 6.5 | 6.75 | 7 | 7.25 |
7.5 | 7.75 | 8 | 8.25 | 8.5 | 8.75 | 9 |
9.25 | 9.75 | 10.25 | 10.75 | 11.25 | 11.75 | 12.25 |
12.75 | 13.75 | 14.75 | 15.75 |
Format | Linear | ||||
Description | Attempts to write values outside of the acceptable range are treated as invalid data – in effect, the ‘cml’ bit in the STATUS_BYTE register and the ‘ivd’ bit in the STATUS_CML register are set, and SMB_ALERT asserted. Additionally, the value of VIN_OFF remains unchanged. Maintaining values within “acceptable range” also indicates that writes to VIN_OFF should not attempt to set its value equal to or higher than that of VIN_ON. | ||||
Default | The default setting results in a real VIN_OFF of 4 V
The default power-up state can be changed using the STORE_USER commands. |
r | r | r | r | r | r | r | r | r | r/wE | r/wE | r/wE | r/wE | r/wE | r/wE | r/wE |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Exponent | Mantissa |
Bits | Field Name | Description |
---|---|---|
7:3 | Exponent | (Format: two's complement)
This is the exponent for the linear format. Default: 11110 (bin) –2 (dec) These default settings are not programmable. Note: Any values written to read-only registers are ignored. |
2:0
7:0 |
Mantissa | (Format: two's complement)
This is the linear format Mantissa. Default: 000 0001 0000 (bin) 16 (dec) (equivalent VIN_OFF voltage = 4 V) Minimum: 000 0001 0000 (bin) 16 (dec) (equivalent VIN_OFF voltage = 4 V) Maximum: 000 0011 1111 (bin) 63 (dec) (equivalent VIN_OFF voltage = 15.75 V) Note: Any values written to read-only registers are ignored. |