SLUSBO6C JANUARY 2014 – October 2018 TPS40425
PRODUCTION DATA.
The VIN_ON command sets the value of the input voltage at which the unit should start power conversion assuming all other conditions are met.
Values written within the supported VIN range are mapped to the nearest supported increment.
The supported VIN_ON values are:
4.25 (default) | 4.5 | 4.75 | 5 | 5.25 | 5.5 | 5.75 |
6 | 6.25 | 6.5 | 6.75 | 7 | 7.25 | 7.5 |
7.75 | 8 | 8.25 | 8.5 | 8.75 | 9 | 9.25 |
9.5 | 10 | 10.5 | 11 | 11.5 | 12 | 12.5 |
13 | 14 | 15 | 16 |
Format | Linear | ||||
Description | Attempts to write values outside of the acceptable range are treated as invalid data – in effect, the ’cml’ bit in the STATUS_BYTE register and the ‘ivd’ bit in the STATUS_CML register are set, and SMB_ALERT asserted. Additionally, the value of VIN_ON remains unchanged. Maintaining values within “acceptable range” also indicates that writes to VIN_ON should not attempt to set its value less than that of VIN_OFF. | ||||
Default | The default setting results in a real VIN_ON of 4.25 V
The default power-up state can be changed using the STORE_USER commands. |
r | r | r | r | r | r | r | r | r | r/wE | r/wE | r/wE | r/wE | r/wE | r/wE | r/wE |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Exponent | Mantissa |
Bits | Field Name | Description |
---|---|---|
7:3 | Exponent | (Format: two's complement)
This is the exponent for the linear format. Default: 11110 (bin) –2 (dec) (equivalent LSB = 0.25 V) These default settings are not programmable. Note: Any values written to read-only registers are ignored. |
2:0
7:0 |
Mantissa | (Format: two's complement)
This is the Mantissa for the linear format. Default: 000 0001 0001 (bin) 17 (dec) (equivalent VIN_ON voltage = 4.25 V) Minimum: 000 0001 0001 (bin) 17 (dec) (equivalent VIN_ON voltage = 4.25 V) Maximum: 000 0100 0000 (bin) 64 (dec) (equivalent VIN_ON voltage = 16 V) Note: Any values written to read-only registers are ignored. |