SLUSFM1 December 2024 TPS4812-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
PIN | TYPE(1) | DESCRIPTION | ||
---|---|---|---|---|
NAME |
TPS48120-Q1 |
TPS48121-Q1 |
||
EN/UVLO |
1 |
1 |
I |
EN/UVLO input. A voltage on this pin above V(UVLOR) 1.21V enables normal operation. If EN/UVLO is below V(UVLOF) then Gate drives are turned OFF. Forcing this pin below V(ENF) 0.3V shuts down the device reducing quiescent current to approximately 1µA (typ). Optionally connect to the input supply through a resistive divider to set the undervoltage lockout. When EN/UVLO is left floating an internal pull down of 100nA pulls EN/UVLO low and keeps the device in OFF state. |
LPM |
2 |
2 |
I |
Mode control input. When driven high, the device enters into active mode. When driven low, the devices enter into low power mode. If low power mode is not required, LPM pin can be tied to EN/UVLO pin. When LPM is left floating an internal pull down of 100nA pulls LPM low. |
INP |
3 |
3 |
I |
Input signal for external FET control. CMOS compatible input reference to GND that sets the state of GATE pin. INP has an internal weak pull down of 100nA to GND to keep GATE pulled to SRC when INP is left floating. |
I_DIR |
4 |
4 |
I |
Open drain I_DIR output. This pin is asserted low by device when current through CS1+ and CS1– flows in reverse direction. |
WAKE |
5 |
5 |
O |
Open drain WAKE output. This pin is asserted low by device when device enters into active mode (when LPM is driven high or when a load wakeup event has occurred). |
FLT |
6 |
6 |
O |
Open drain fault output. FLT goes low during charge pump UVLO, Main FET SCP, I2t timer trigger, NTC based external FET overtemperature fault. This pin asserts low after the voltage on the I2t pin has reached the fault threshold of 2V. This pin indicates the main FET is about to turn off due to an overload condition. This pin asserts low along with GATE turn off during short-circuit. The FLT pin does not go to a high impedance state until the overcurrent condition and the auto-retry time expire. |
TMR |
7 |
7 |
I |
Auto-retry or latch timer input after overcurrent fault. A capacitor across TMR pin to GND sets the times for retry periods. Leave open for fastest setting. Connect resistor across CTMR from TMR pin to GND for latch-off functionality. |
GND |
8 |
8 |
G |
Connect GND to system ground. |
IMON |
9 |
9 |
O |
Analog bi-directional current monitor output. This pin sources a scaled down ratio of current through the external current sense resistor RSNS. A resistor from this pin to GND converts current proportional to voltage. If unused, leave floating or can be connected to ground. |
ITMPO |
10 |
10 |
O |
Analog temperature output. Analog voltage feedback provides a voltage proportional to thermistor temperature. If unused, leave floating. |
IOC |
11 |
— |
I |
Overcurrent detection setting. A resistor across IOC to GND sets the over current comparator threshold. IOC pin can also be driven externally using MCU. |
N.C. |
— |
11 |
— |
No connect. |
I2t |
12 |
— |
O |
I2t timer input. A capacitor across I2t pin to GND sets the times for overcurrent (tOC). |
N.C. |
— |
12 |
— |
No connect. |
G |
13 |
13 |
O |
Gate of external bypass FET. 100µA peak source and 0.39A sink capacity. Connect to the gate of the external bypass FET. |
BST |
14 |
14 |
O |
High side bootstrapped supply. An external capacitor with a minimum value of 0.1µF should be connected between this pin and SRC. Voltage swing on this pin is 12V to (VIN + 12V). |
SRC |
15 |
15 |
O |
Source connection of the external FET. |
GATE |
16 |
16 |
O |
High current gate driver pull-up and pull-down. 0.5A peak source and 2A sink capacity. This pin pulls GATE up to BST and down to SRC. For the fastest tun-on and turn-off, tie this pin directly to the gate of the external high side MOSFET in main path. |
TMP |
18 |
18 |
I |
Temperature input. Analog connection to external NTC thermistor Connect TMP pin directly to VS if this feature is not used |
CS1– |
19 |
19 |
I |
Main path current sense negative input. Connect a resistor (RSETR) across CS1– to the external current sense resistor to set IMON gain in reverse direction. |
CS1+ |
20 |
20 |
I |
Main path current sense positive input. Connect a resistor (RSETF) across CS1+ to the external current sense resistor to set IMON gain in forward direction. Connect CS1+ and CS1– to VBATT if main FET current sensing is not used. |
ISCP |
21 |
21 |
I |
Short-circuit detection threshold setting. Connect ISCP to DRN if short-circuit protection is not desired. |
VS |
22 |
22 |
P |
Supply pin of the controller. |
CS2– |
23 |
23 |
I |
Bypass path current sense negative input. |
DRN |
24 |
24 |
I |
Main path SCP sense negative input. Connect DRN+ and CS2– together to VBATT after RSNS if bypass path is not used. |
GND |
Thermal Pad |
— |
— |
Connect exposed thermal pad to GND plane. |