SLVSCT3 March 2015 TPS51275B-1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS51275B-1 device is typically used as a dual-synchronous buck controller, which converts an input voltage ranging from 5 to 24 V, to output voltage of 5 V and 3.3 V (respectively). The device is targeted for power-supply solutions for notebook and desktop computer systems.
For this design example, use the parameters listed in Table 2.
PARAMETER | VALUE |
---|---|
Input voltage range | 5.5 to 24 V |
Channel 1 output voltage | 5 V |
Channel 1 output voltage | 8 A |
Channel 2 output voltage | 3.3 V |
Channel 2 output voltage | 8 A |
The external components selection is relatively simple for a design using D-CAP mode. Table 3 lists the key external components that are recommended for this application design (see Figure 18).
REFERENCE DESIGNATOR |
FUNCTION | MANUFACTURER | PART NUMBER |
---|---|---|---|
L1 | Output Inductor (5 VOUT) | Alps | GLMC3R303A |
L2 | Output Inductor (3.3 VOUT) | Alps | GLMC2R203A |
C1 | Output Capacitor (5 VOUT) | SANYO | 6TPE220MAZB × 2 |
C2 | Output Capacitor (3.3 VOUT) | SANYO | 6TPE220MAZB × 2 |
Q1 | MOSFET (5 VOUT) | TI | CSD87330Q3D |
Q2 | MOSFET (3.3 VOUT) | TI | CSD87330Q3D |
The recommended value of R2 is between 10 kΩ and 20 kΩ. Use Equation 5 to calculate the value of R1.
The inductance value should be determined to give the ripple current of approximately ½ to ¼ of maximum output current and less than half of OCL (valley) threshold. A larger ripple current increases the output ripple voltage, improves signal-to-noise ratio, and helps ensure stable operation.
The calculated inductance for channel1 and channel2 is 3.3 µH and 2 µH, respectively. For this design, select the inductance values of 3.3 µH and 2.2 µH for these two channels.
The inductor must also have low DCR to achieve good efficiency, as well as enough room above the peak inductor current before saturation. Use Equation 7 to calculate the peak inductor current.
Organic semiconductor capacitors or specialty polymer capacitors are recommended. Determine the ESR to meet the required ripple voltage. Use Equation 8 to quickly calculate the ESR.
where
The calculated minimum-required ESR for channel1 and channel2 is 9.9 mΩ and 7.8 mΩ, respectively. For this design, use two 220-µF, 35-mΩ polymer capacitors in parallel for each channel. The equivalent ESR is 17.5 mΩ which meets the minimum ESR requirement. Using a value of 440 µF for the output capacitor and 17.5 mΩ of ESR, the resulting value of the 0-dB frequency, f0 (see Equation 4), is approximately 21 kHz which is much less than fSW / 4 for both channels.
IOUT1 = 0 to 3 A | IOUT2 = 0 A | VVIN = 7.4 V |
IOUT1 = 0 A | IOUT2 = 0 to 3 A | VVIN = 7.4 V |