SLUSFR0A July 2024 – August 2024 TPS51375
PRODUCTION DATA
The VCC pin is the output of the internal 5V linear regulator that creates the bias for all the internal circuitry and MOSFET gate drivers. The VCC pin must be bypassed with a 2.2µF capacitor. The UVLO circuit monitors the VCC pin voltage and disables the output when VCC falls below the UVLO threshold.
An external voltage that is connected to the BYP pin can override the internal LDO, switching to the external rail after a higher voltage is detected. This action enhances the efficiency of the converter because the quiescent current now runs off this external rail instead of the input power supply. This BYP external voltage must come after VIN voltage on and quit before VIN off.
The devices is integrated with a VCC switchover function which supports connecting the BYP pin to VOUT directly if the VOUT is set to higher than 4.8V. The VCC switchover function is designed to bypass internal 5V LDO with the power from VOUT. The VCC switchover is a seamless behavior of regulator and does not need any additional configuration.
The VCC pin switchover function is asserted when three conditions are present:
In this switchover condition, one thing occurs: the VCC output is connected to VOUT by internal switchover MOSFET.