SLUSFR0A July 2024 – August 2024 TPS51375
PRODUCTION DATA
The advanced Eco-mode control schemes to maintain high light load efficiency. As the output current decreases from heavy load conditions, the inductor current is also reduced and eventually comes to a point where the rippled valley touches zero level, which is the boundary between continuous conduction and discontinuous conduction modes. The rectifying MOSFET is turned off when the zero inductor current is detected. As the load current further decreases, the converter runs into discontinuous conduction mode. The on-time is kept almost the same as in continuous conduction mode so that discharging the output capacitor with smaller load current to the level of the reference voltage takes longer. This action makes the switching frequency lower, proportional to the load current, and keeps the light load efficiency high. Use Equation 2 to calculate the light load current where the transition to Eco-mode operation happens (IOUT(LL)).
After identifying the application requirements, design the output inductance (LOUT) so that the inductor peak-to-peak ripple current is approximately between 20% and 40% of IOUT(ma×) (peak current in the application). Sizing the inductor properly so that the valley current does not hit the negative low-side current limit is important.