SLVSBF0C JULY 2012 – April 2019 TPS53015
PRODUCTION DATA.
The TPS53015 device has a cycle-by-cycle over current limit feature. The over current limits the inductor valley current by monitoring the voltage drop across the low-side MOSFET RDS(on) during the low-side driver on-time. If the inductor current is larger than the overcurrent limit (OCL), the device delays the start of the next switching cycle until the sensed inductor current falls below the OCL current. MOSFET RDS(on) current sensing is used to provide an accuracy and cost effective solution without external devices. To program the OCL, a resister should be connected between DRVL and PGND. The recommended values are given inTable 1.
Resistor Value ( kΩ) | VTRIP (V) |
6.8 | 0.050 |
11 | 0.087 |
18 | 0.125 |
27 | 0.174 |
39 | 0.224 |
56 | 0.274 |
75 | 0.336 |
Use Equation 1 to calculate IOCL.
The trip voltage is set between 0.05 V to 0.336 V over all operational temperature, including the 4000ppm/°C temperature slope compensation for the temperature dependency of the RDS(on). If the load current exceeds the overcurrent limit, the voltage begins to drop. If the overcurrent conditions continues the output voltage falls below the undervoltage protection threshold and the device shuts down.