SLUSAE5G August 2011 – April 2021 TPS53355
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
TPS53355 has cycle-by-cycle overcurrent limiting control. The inductor current is monitored during the OFF state and the controller maintains the OFF state during the period in that the inductor current is larger than the overcurrent trip level. In order to provide both good accuracy and cost effective solution, TPS53355 supports temperature compensated MOSFET RDS(on) sensing. The TRIP pin should be connected to GND through the trip voltage setting resistor, RTRIP. The TRIP terminal sources current (ITRIP) which is 10 μA typically at room temperature, and the trip level is set to the OCL trip voltage VTRIP as shown in Equation 1.
The inductor current is monitored by the LL pin. The GND pin is used as the positive current sensing node and the LL pin is used as the negative current sense node. The trip current, ITRIP has 4700ppm/°C temperature slope to compensate the temperature dependency of the RDS(on).
As the comparison is made during the OFF state, VTRIP sets the valley level of the inductor current. Thus, the load current at the overcurrent threshold, IOCP, can be calculated as shown in Equation 2.
In an overcurrent or short circuit condition, the current to the load exceeds the current to the output capacitor thus the output voltage tends to decrease. Eventually, it crosses the undervoltage protection threshold and shuts down. After a hiccup delay (16 ms with 0.7 ms sort-start), the controller restarts. If the overcurrent condition remains, the procedure is repeated and the device enters hiccup mode.
Hiccup time calculation:
where
SELECTED SOFT-START TIME (tSS) (ms) | n | HICCUP WAIT TIME (tHIC(wait)) (ms) | HICCUP DELAY TIME (tHIC(dly)) (ms) |
---|---|---|---|
0.7 | 8 | 2.052 | 14.364 |
1.4 | 9 | 3.076 | 21.532 |
2.8 | 10 | 5.124 | 35.868 |
5.6 | 11 | 9.220 | 64.540 |