SLVS889C October 2008 – November 2014 TPS54140
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | ||
---|---|---|---|---|
NO. | NAME | |||
1 | BOOT | O | A bootstrap capacitor is required between the BOOT and PH pins. If the voltage on this capacitor is below the minimum required by the device, the output is forced to switch off until the capacitor is refreshed. | |
2 | VIN | I | This pin is the 3.5- to 42-V input supply voltage. | |
3 | EN | I | This pin is the enable pin and internal pullup current source. To disable, pull below 1.2 V. Float this pin to enable. Adjust the input undervoltage lockout with two resistors. | |
4 | SS/TR | I | This pin is the slow-start and tracking pin. An external capacitor connected to this pin sets the output rise time. Because the voltage on this pin overrides the internal reference, it can be used for tracking and sequencing. | |
5 | RT/CLK | I | This pin is the resistor timing and external clock pin. An internal amplifier holds this pin at a fixed voltage when using an external resistor to ground to set the switching frequency. If the pin is pulled above the PLL upper threshold, a mode change occurs and the pin becomes a synchronization input. The internal amplifier is disabled and the pin is a high impedance clock input to the internal PLL. If clocking edges stop, the internal amplifier is re-enabled and the mode returns to a resistor set function. | |
6 | PWRGD | O | This pin is an open drain output. This pin is asserted low if the output voltage is low because of thermal shutdown, dropout, overvoltage, or EN shut down. | |
7 | VSENSE | I | This pin is the inverting node of the transconductance (gm) error amplifier. | |
8 | COMP | O | This pin is the error amplifier output and input to the output-switch current comparator. Connect frequency compensation components to this pin. | |
9 | GND | — | Ground pin | |
10 | PH | O | This pin is the source of the internal high-side power MOSFET. | |
11 | Thermal Pad | — | The GND pin must be electrically connected to the exposed pad on the printed circuit board for proper operation. |