SNVSAZ4A February 2021 – March 2021 TPS541620
PRODUCTION DATA
The SS pin is used to program different soft-start times in multi-phase mode. In dual-output mode, an internally fixed soft start is used.
This is useful if a load has specific timing requirements for the output voltage of the regulator. A longer soft-start time is also useful if the output capacitance is very large and would require large amounts of current to quickly charge the output capacitors to the output voltage level. The large currents necessary to charge the capacitor can reach the current limit or cause the input voltage rail to sag due excessive current draw from the input power supply. Limiting the output voltage slew rate solves both of these problems. The example design has the soft-start time set to 2.5 ms.