SLVS412F December 2001 – April 2019 TPS54310
PRODUCTION DATA.
The output voltage of the TPS54310 can be set by feeding back a portion of the output to the VSENSE pin using a resistor divider network. In the application circuit of Figure 10, this divider network is comprised of resistors R5 and R4. To calculate the resistor values to generate the required output voltage use Equation 4.
Start with a fixed value of R5 and calculate the required R4 value. Assuming a fixed value of 10 kΩ for R5, the following table gives the appropriate R4 value for several common output voltages:
OUTPUT VOLTAGE (V) | R4 VALUE (KΩ) |
---|---|
1.2 | 28.7 |
1.5 | 14.7 |
1.8 | 9.76 |
2.5 | 5.49 |
3.3 | 3.74 |