SLVS946E September 2009 – April 2018 TPS54418
PRODUCTION DATA.
The TPS54418 device uses a transconductance amplifier for the error amplifier and readily supports two of the commonly used frequency compensation circuits. The compensation circuits are shown in Figure 34. The Type-II circuits are most likely implemented in high bandwidth power supply designs using low ESR output capacitors. In Type-IIA, one additional high frequency pole is added to attenuate high-frequency noise.
The design guidelines for TPS54418 device loop compensation are as follows:
where