SLVS834B July 2008 – June 2019 TPS5450-Q1
PRODUCTION DATA.
The design equations given in the example circuit can be used to generate circuits using the TPS5450-Q1. These designs are based on certain assumptions and will tend to always select output capacitors within a limited range of ESR values. If a different capacitor type is desired, it may be possible to fit one to the internal compensation of the TPS5450-Q1. Equation 15 gives the nominal frequency response of the internal voltage-mode type III compensation network:
where
Using this information along with the desired output voltage, feed forward gain and output filter characteristics, the closed loop transfer function can be derived.