SLUSF27 November 2023 TPS546B24S
PRODUCTION DATA
The BP1V5 pin requires a minimum capacitance of 1 μF connected to DRTN. The VDD5 pin must have approximately 4.7 μF of capacitance connected to PGND. The AVIN pin must have approximately 1 μF of capacitance connected to AGND. To filter switching noise on the AVIN pin, a small value resistor of typically 10-Ω is recommended to be placed between PVIN and AVIN. If using split rail inputs and if the AVIN pin is connected to the VDD5 pin, a small value resistor is recommended to be placed between AVIN and VDD5.