SLUSF26 March 2023 TPS546D24S
PRODUCTION DATA
Use Equation 9 to calculate the value of the output inductor (L) for each phase. The current is shared between each phase so the output current used in this calculation is divided by the number of phases.
Selecting a value of 0.3 for the KIND coefficient, the target inductance, L, is 120 nH. An inductance of 150 nH is selected. Use Equation 10, Equation 11, and Equation 12 to calculate the inductor-ripple current (IRIPPLE), RMS current (IL(rms)), and peak current (IL(peak)), respectively. The resulting values are IRIPPLE = 9.2 A, IL(rms) = 40.1 A and IL(peak) = 44.6 A. Use these values to select an inductor with approximately the target inductance value and current ratings that allow normal operation with some margin.
Considering the required inductance, RMS current and peak current, the 150-nH inductor, SLC1480-151ML, from Coilcraft was selected for this application.