SLUSF26 March 2023 TPS546D24S
PRODUCTION DATA
Only the loop controller device (U1) needs a resistor divider at the ADRSEL pin. In this example the ADRSEL pin is left floating. This sets the PMBus device address to the EEPROM value, 0x24h (36d) by default, and the SYNC pin to auto detect with 0 degrees phase shift. Use the following tables, Table 7-14 and Table 7-15, to select the resistor to AGND code and resistor divider code needed for the desired configuration.