SLVSDC9B November 2016 – November 2019 TPS54824
PRODUCTION DATA.
Figure 55 through Figure 58 shows an alternate example PCB layout with unsymmetrical placement of the input capacitors and output capacitors. Both VIN pins are still bypassed to their adjacent PGND pins with an input capacitor placed as close as possible to the IC. When using this alternate layout, CI2 should be increased to 1 µF.