SLVSD46A November 2017 – December 2021 TPS55160-Q1 , TPS55162-Q1 , TPS55165-Q1
PRODUCTION DATA
PIN | I/O(1) | TYPE(2) | DESCRIPTION | |
---|---|---|---|---|
NAME | NO. | |||
PGND | 1 | — | G | Power-ground pin |
L1 | 2 | I | A | Buck power-stage switch node. Connect an inductor with a nominal value of 4.7 µH between the L1 and L2 pins. |
BST1 | 3 | I | A | Bootstrap node for the buck power stage. Connect a 100-nF capacitor between this pin and the L1 pin. |
VINP | 4 | — | P | Supply-power input voltage. Connect this pin to the input supply line. |
VINL | 5 | — | P | Supply-input voltage for internal biasing. Connect this pin to the input supply line. |
IGN | 6 | I | D | Ignition-enable input signal. The ignition is enabled when this pin is high (1) and is disabled when this pin is low (0). |
PS | 7 | I | D | Logic-level input signal to enable and disable low-power mode. The power mode is low-power mode when this pin is high (1) and is normal mode when this pin is low (1). |
IGN_PWRL | 8 | I | D | Logic-level IGN power-latch signal. The IGN pin is latched when this pin is high (1) and is not latched when this pin is low (0). |
SS_EN | 9 | I | D | Configuration pin to enable and disable the spread-Spectrum. The spread-spectrum feature is enabled when this pin is open and disabled when this pin is low. |
PG_DLY | 10 | I | A | Configuration pin for power-good delay time. Connect this pin to a resistor with a value from 10kΩ to 100kΩ to configure the PG delay time from 0.5 ms to 40 ms. Connect this pin to ground for the default PG delay time which is 2 ms (typical). |
VREG_Q(3) | 11 | I | A | Quiet feedback pin for the gate-drive supply of the buck-boost power stages. This pin must be connected close to the top side of the 4.7-µF (typical) decoupling capacitor at the VREG output pin. |
VREG | 12 | O | A | Gate-drive supply for the buck-boost power stages. Apply a 4.7-µF (typical) decoupling capacitor at this pin to the power ground. The VREG pin cannot drive external loads in the application. |
GND | 13 | — | G | Analog ground |
VOS_FB | 14 | I | A | For the TPS55160-Q1 and TPS55162-Q1 devices, this pin is used to
adjust the VOUT configuration. Connect this pin to a resistive
feedback network with less than 1-MΩ total resistance between the
VOUT pin, FB pin, and GND pin (analog ground). For the TPS55165-Q1 device, this pin is used to select the output voltage. The output voltage is set to 5 V when this pin is connected to the GND pin. The output voltage is 12 V when this pin is connected to the VREG pin. |
PG | 15 | O | D | Output power good pin. This pin is an open-drain pin. The status of the power-good output is good when this pin is high (1) and has a failure when this pin is low (0) |
VOUT_SENSE | 16 | I | A | Sense pin for the buck-boost converter output voltage. This pin must be connected to the VOUT pin. |
VOUT | 17 | O | A | Buck-boost converter output voltage |
GND | 18 | — | G | Analog ground |
BST2 | 19 | I | A | Bootstrap node for the boost power-stage. Connect a typical 100-nF capacitor between this pin and the L2 pin. |
L2 | 20 | I | A | Boost power-stage switch node. Connect an inductor with a nominal value of 4.7 µH between the L1 and L2 pins. |
PowerPAD | — | — | The thermal pad must be soldered to the power ground to achieve the appropriate power dissipation through the analog ground plane. |