SLVSBV5C June 2014 – September 2021 TPS55340-Q1
PRODUCTION DATA
The input-to-output voltage-conversion ratio of the TPS55340-Q1 device is limited by the worst-case maximum duty cycle of 89% and the minimum duty cycle, which is determined by the minimum on time of 77 ns and the switching frequency. Use Equation 9 to calculate the minimum duty cycle. Selecting a 600-kHz switching frequency, the minimum duty cycle is calculated as 4%.
The duty cycle at which the converter operates is dependent on the mode in which the converter is running. If the converter is running in Discontinuous conduction mode (DCM) where the inductor current ramps to zero at the end of each cycle, the duty cycle varies with changes of the load much more than when running in Continuous conduction mode (CCM). In Continuous conduction mode where the inductor maintains a minimum DC current, the duty cycle is related primarily to the input and output voltages as calculated with Equation 10. Assume a 0.5-V drop (V(D)) across the Schottky rectifier. At the minimum input of 5 V, the duty cycle is 80%. At the maximum input of 12 V, the duty cycle is 51%.
At light loads, the converter operates in DCM. In this case, the duty cycle is a function of the following, as calculated in Equation 11:
The light-load duty cycle can be calculated only after an inductance is selected (see Section 8.2.1.2.4). While operating in DCM with very-light load conditions, the duty cycle demand forces the TPS55340-Q1 device to operate with the minimum on time. The converter then begins pulse skipping, which can increase the output ripple.
All converters using a diode as the freewheeling or catch component have a load-current level at which the converters transition from DCM to CCM. The transit from DCM to CCM is the point when the inductor current falls to zero during the off time of the power switch. At higher load currents, the inductor current does not fall to zero and the diode and switch current assume a trapezoidal wave-shape as opposed to a triangular wave-shape. The load current boundary between discontinuous conduction and continuous conduction is calculated for a set of converter parameters as shown in Equation 12.
where
For loads higher than the result of the Equation 12, the duty cycle is given by Equation 10. For loads less than the results of Equation 12, the duty cycle is given Equation 11.
Unless otherwise stated, the design equations that follow assume that the converter is running in Continuous conduction mode, which typically results in a higher efficiency for the power levels of this converter.