SLVSH62 November 2023 TPS61033-Q1 , TPS610333-Q1
PRODUCTION DATA
The TPS61033-Q1 uses a valley current limit sensing scheme. Current limit detection occurs during the off-time by sensing of the voltage drop across the synchronous rectifier.
When the load current is increased such that the inductor current is above the current limit within the whole switching cycle time, the off-time is increased to allow the inductor current to decrease to this threshold before the next on-time begins (so called frequency foldback mechanism). When the current limit is reached, the output voltage decreases during further load increase.
The maximum continuous output current (IOUT(LC)), before entering current limit (CL) operation, can be defined by Equation 2.
where
The duty cycle can be estimated by Equation 3.
where
The peak-to-peak inductor ripple current is calculated by Equation 4.
where