SLVSH62 November 2023 TPS61033-Q1 , TPS610333-Q1
PRODUCTION DATA
There are two ways to set the output voltage of the TPS61033-Q1: adjustable or fixed. If the FB is connected to VIN, the TPS61033-Q1 works as a fixed 5.0-V output voltage version, the TPS61033-Q1 uses the internal resistor divider.
The output voltage is also can be set by an external resistor divider (R1, R2 in Figure 8-1). When the output voltage is regulated, the typical voltage at the FB pin is VREF. Thus the resistor divider is determined by Equation 5.
where
TPS610333-Q1 can only support fixed 5.0-V output voltage, so engineer needs to connected FB pin to VIN pin rather than external resistor divider