SLVSD38C November 2015 – August 2021 TPS61089
PRODMIX
The peak input current is set by selecting the correct external resistor value correlating to the required current limit. Use Equation 4 to calculate the correct resistor value:
where
For a typical current limit of 8 A, the resistor value is 127 kΩ. Considering the device variation and the tolerance over temperature, the minimum current limit at the worst case can be 0.8 A lower than the value calculated by Equation 4. The minimum current limit must be higher than the required peak switch current at the lowest input voltage and the highest output power to make sure the TPS61089x does not hit the current limit and still can regulate the output voltage in these conditions.