SLVSHB5A October 2024 – November 2024 TPS61287
PRODUCTION DATA
The bootstrap capacitor between the BOOT and SW pin supplies the gate current to charge the high-side FET device gate during the turn on of each cycle. The gate current also supplies charge for the bootstrap capacitor. The recommended value of the bootstrap capacitor is 0.1μF to 1.0μF. CBOOT must be a good quality, low-ESR ceramic capacitor located at the pins of the device to minimize potentially damaging voltage transients caused by trace inductance.
The VCC pin is the output of the internal LDO. A ceramic capacitor of more than 2.2μF is required at the VCC pin to get a stable operation of the LDO.