With the small signal models coming out, the next step is to calculate the compensation network parameters with the given inductor and output capacitance.
- Set the Crossover Frequency, ƒC.
- The first step is to set the loop crossover
frequency, ƒC. The higher crossover frequency, the faster the
loop response is. It is generally accepted that the loop gain cross over
no higher than the lower of either 1/10 of the switching frequency,
ƒSW, or 1/5 of the RHPZ frequency, ƒRHPZ. Then
calculate the loop compensation network values of Rc,
Cc, and Cp in following sections.
- Set the Compensation Resistor, RC.
- By placing ƒZ below ƒC,
for frequencies above ƒC, RC | | REA
approximately = RC, so RC × GEA sets
the compensation gain. Setting the compensation gain,
KCOMP-dB, at ƒZ, results in the total loop
gain, T(s) = GPS(s) × HEA(s) × He(s)
being zero at ƒC.
- Therefore, to approximate a single-pole rolloff
up to fP2, rearrange Equation 19 to solve for RC so that the compensation gain, KEA, at
fC is the negative of the gain, KPS, read at
frequency fC for the power stage bode plot or more simply:
Equation 19. ![GUID-CE56D9A4-04A6-4B46-A131-EBB6DB2B6AFB-low.gif](/ods/images/SLVSEE7B/GUID-CE56D9A4-04A6-4B46-A131-EBB6DB2B6AFB-low.gif)
where
- KEA is
gain of the error amplifier network
- KPS is
the gain of the power stage
- GEA is
the transconductance of the amplifier, the typical value of
GEA = 175 µA / V
- Set the compensation zero capacitor, CC.
- Place the compensation zero at the power stage
pole position of ROUT, COUT to get:
Equation 20. ![GUID-85096E82-EA16-4B51-BDE0-0FF75116D1F8-low.gif](/ods/images/SLVSEE7B/GUID-85096E82-EA16-4B51-BDE0-0FF75116D1F8-low.gif)
- Set ƒZ = ƒP, and get:
Equation 21. ![GUID-DD763818-B5F8-4C16-8526-553ADA1CB92F-low.gif](/ods/images/SLVSEE7B/GUID-DD763818-B5F8-4C16-8526-553ADA1CB92F-low.gif)
- Set the compensation pole capacitor, CP.
- Place the compensation pole at the zero produced
by the RESR and the COUT. It is useful for
canceling unhelpful effects of the ESR zero.
Equation 22. ![GUID-7F76CA94-DBE7-4828-97F1-5AA63A1F5AE1-low.gif](/ods/images/SLVSEE7B/GUID-7F76CA94-DBE7-4828-97F1-5AA63A1F5AE1-low.gif)
Equation 23. ![GUID-2325C3AC-2C1F-42C9-B1BC-0D7FE420ACF4-low.gif](/ods/images/SLVSEE7B/GUID-2325C3AC-2C1F-42C9-B1BC-0D7FE420ACF4-low.gif)
- Set ƒP2 = ƒESR, and get:
Equation 24. ![GUID-1A1A24D5-76D1-4660-BC1D-1BFF20D3D742-low.gif](/ods/images/SLVSEE7B/GUID-1A1A24D5-76D1-4660-BC1D-1BFF20D3D742-low.gif)
- If the calculated value of CP is less
than 10 pF, it can be neglected.
Designing the loop for greater than 45° of phase margin and greater than
6-dB gain margin eliminates output voltage ringing during the line and load
transient. The RC = 61.9 kΩ , CC = 680 pF for this design
example.