SLVSEE7B June 2018 – January 2021 TPS61372
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
A boost converter normally requires two main passive components for storing the energy during power conversion: an inductor and an output capacitor. The inductor affects the steady state efficiency (including the ripple and efficiency) as well as the transient behavior and loop stability, which makes the inductor to be the most critical component in application.
When selecting the inductor, as well as the inductance, the other parameters of importance are:
Choosing the inductor ripple current with the low ripple percentage of the average inductor current results in a larger inductance value, maximizes the potential output current of the converter, and minimizes EMI. The larger ripple results in a smaller inductance value and a physically smaller inductor, which improves transient response, but results in potentially higher EMI.
The rule of thumb in choosing the inductor is to make sure the inductor ripple current (ΔIL) is a certain percentage of the average current. The inductance can be calculated by Equation 2, Equation 3, and Equation 4:
where
The current flowing through the inductor is the inductor ripple current plus the average input current. During power up, load faults, or transient load conditions, the inductor current can increase above the peak inductor current calculated.
Inductor values can have ±20% or even ±30% tolerance with no current bias. When the inductor current approaches the saturation level, its inductance can decrease 20% to 35% from the value at 0-A bias current depending on how the inductor vendor defines saturation. When selecting an inductor, make sure its rated current, especially the saturation current, is larger than its peak current during the operation.
The inductor peak current varies as a function of the load, the switching frequency, and the input and output voltages and it can be calculated by Equation 5 and Equation 6.
where
The input DC current is determined by the output voltage, the output current, and efficiency can be calculated by:
where
While the inductor ripple current depends on the inductance, the frequency, the input voltage, and duty cycle calculated by Equation 2, replace Equation 2, Equation 6 into Equation 5 to calculate the inductor peak current:
where
The heat rating current (RMS) is calculated by Equation 8:
where
It is important that the peak current does not exceed the inductor saturation current and the RMS current is not over the temperature related rating current of the inductors.
For a given physical inductor size, increasing inductance usually results in an inductor with lower saturation current. The total losses of the coil consists of the DC resistance ( DCR ) loss and the following frequency dependent loss:
For a certain inductor, the larger current ripple (smaller inductor) generates the higher DC and frequency-dependent loss. An inductor with lower DCR is basically recommended for higher efficiency. However, it is usually a tradeoff between the loss and footprint.
The following inductor series in Table 8-2 from the different suppliers are recommended.
PART NUMBER | L (μH) | DCR Typ (mΩ) TYP. | SATURATION CURRENT / TYP. | SIZE (L × W × H mm) | VENDOR(1) |
---|---|---|---|---|---|
XAL4020-222ME | 2.2 | 35 | 5.6 | 4 x 4 x 2 | Coilcraft |
DFE322512F-2R2M=P2 | 2.2 | 66 | 2.6 | 3.2 x 2.5 x 1.2 | Murata |
DFE322520FD-4R7M# | 4.7 | 98 | 3.4 | 3.2 x 2.5 x 2.0 | Murata |