SLVSEE7B June 2018 – January 2021 TPS61372
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The output capacitor is mainly selected to meet the requirements at load transient or steady state. Then the loop is compensated for the output capacitor selected. The output ripple voltage is related to the equivalent series resistance (ESR) of the capacitor and its capacitance. Assuming a capacitor with zero ESR, the minimum capacitance needed for a given ripple can be calculated by Equation 9:
where
The additional output ripple component caused by ESR is calculated by Equation 10:
where
For the ceramic capacitor, the ESR ripple can be neglected. However, for the tantalum or electrolytic capacitors, it must be considered if used.
Care must be taken when evaluating the rating of a ceramic capacitor under the DC bias. Ceramic capacitors can derate by as much as 70% of its capacitance at its rated voltage. Therefore, enough margins on the voltage rating should be considered to ensure adequate capacitance at the required output voltage.
PART NUMBER | C (μF) | PIECES | DESCRIPTION | SIZE | VENDOR(1) |
---|---|---|---|---|---|
GRM188R61E106MA73D | 10 | 3 | X5R, 0603, 5 V, ±20% tolerance | 0603 | Murata |