SLVS764G June 2007 – April 2018 TPS62290 , TPS62291 , TPS62293
PRODUCTION DATA.
The output voltage can be calculated to:
with an internal reference voltage VREF typical 0.6 V.
To minimize the current through the feedback divider network, R2 should be 180 kΩ or 360 kΩ. The sum of R1 and R2 should not exceed ~1MΩ, to keep the network robust against noise.
An external feed forward capacitor C1 is required for optimum load transient response. The value of C1 should be in the range between 22 pF and 33 pF.
Route the FB line away from noise sources, such as the inductor or the SW line.