SLVSH51A July 2023 – January 2025 TPS631012 , TPS631013
PRODUCTION DATA
The inductor selection is affected by several parameters such as the following:
See Table 8-2 for typical inductors.
For high efficiencies, the inductor with a low DC resistance is needed to minimize conduction losses. Especially at high-switching frequencies, the core material has a high impact on efficiency. When using small chip inductors, the efficiency is reduced mainly due to higher inductor core losses. Core losses need to be considered when selecting the appropriate inductor. The inductor value determines the inductor ripple current. The larger the inductor value, the smaller the inductor ripple current and the lower the conduction losses of the converter. Conversely, larger inductor values cause a slower load transient response. To avoid saturation of the inductor, the peak current for the inductor in steady state operation is calculated using Equation 2. Only the equation that defines the switch current in boost mode is shown because this provides the highest value of current and represents the critical current value for selecting the right inductor.
where:
The calculation must be done for the minimum input voltage in boost mode.
Calculating the maximum inductor current using the actual operating conditions gives the minimum saturation current of the inductor needed. It is recommended to choose an inductor with a saturation current 20% higher than the value calculated using Equation 2. Possible inductors are listed in Table 8-2.
INDUCTOR VALUE [µH] | SATURATION CURRENT [A] | DCR [mΩ] | PART NUMBER | MANUFACTURER(1) | SIZE (L × W × H mm) |
---|---|---|---|---|---|
1 | 4.3 | 42 | DFE252012P-1R0M=P2 | MuRata | 2.5 × 2.0 × 1.2 |
1 | 4.2 | 43 | HTEK20161T-1R0MSR | Cyntec | 2.0 × 1.6 × 1.0 |
1 | 2.2 | 75 | MAKK2016T1R0M (2) | Taiyo Yuden | 2.0 × 1.6 × 1.0 |
1 | 2.0 | 144 | DFE18SAN1R0ME0 (2) | Murata | 1.6 × 0.8 × 0.8 |