SLVS950I July 2009 – May 2018 TPS65070 , TPS65072 , TPS65073 , TPS650731 , TPS650732
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
INT | B7 | B6 | B5 | B4 | B3 | B2 | B1 | BO |
---|---|---|---|---|---|---|---|---|
Bit name and function | MASK
AC/USB |
MASK TSC | MASK
PB_IN |
TSC INT | PB_IN
INT |
USB or AC input voltage applied | USB or AC input voltage removed | |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Set by signal | Cleared when read | Cleared when read | Cleared when read | Cleared when read | ||||
Default value loaded by: | UVLO | UVLO | UVLO | UVLO | UVLO | UVLO | UVLO | |
Read/write | R/W | R/W | R/W | R | R | R | R | R |
Bit 7 | MASK AC/USB
0 = no interrupt generated if voltage at AC or USB is applied or removed 1 = the pin INT is actively pulled low if one of the Bits 1 to Bit 0 are 1 |
Bit 6 | MASK TSC
0 = no interrupt generated if the touch screen is detecting a “touch” 1 = the pin INT is actively pulled low if a “touch” on the touch screen is detected |
Bit 5 | MASK PB_IN
0 = no interrupt generated if the PB_IN is pulled low. 1 = the pin INT is actively pulled low if PB_IN was pulled low. |
Bit 3 | TSC INT
0 = no “touch” on the touch screen detected 1 = “touch” detected and the Bit has not been read ever since |
Bit 2 | PB_IN INT
0 = PB_IN not active 1 = PB_IN is actively pulled low (or high optionally) and the Bit has not been read ever since |
Bit 1 | USB or AC INPUT VOLTAGE APPLIED
0 = no change (voltage still applied or never applied) 1 = voltage at USB or AC has been applied and the Bit has not been read ever since |
Bit 0 | USB or AC INPUT VOLTAGE REMOVED
0 = no change (voltage still applied or never applied) 1 = the voltage at USB or AC has been removed and the Bit has not been read ever since |