Connect the LDO5V output to the
DRV5V_x_x inputs for situations where an external 5-V supply is not initially
available or is not available the entire time PMIC is on. If the external 5-V
supply is always present, then DRV5V_x_x can be directly connected to remove the
V5ANA-to-LDO5P0 load switch RDSON.
Ensure that none of the control
pins are potentially floating.
Include 0-Ω resistors on the DRVH
and BOOT pins of controllers on prototype boards, which allows for slowing the
controllers if the system is unable to handle the noise generated by the large
switching or if switching voltage is too large due to layout.
Do not connect the V5ANA power
input to a different source other than PVINx. A mismatch here causes reference
circuits to regulate incorrectly.
Do not supply the V5ANA power
input before the VSYS. Reference biasing of the internal FETs may turn on the HS
FET and pass the input to the output until VSYS is biased.