SLVSCQ9E November 2014 – March 2022 TPS65400
PRODUCTION DATA
The STORE_DEFAULT_ALL command saves the PMBus parameters from operating memory into the default store in data flash (EEPROM). The TPS65400 uses the most recently written set of default store values at startup. The maximum time it takes for the data flash to be written is 70 ms.
This command has no PAGE support.
The OPERATION, PAGE, and WRITE_PROTECT parameters are not stored in the default store in data flash.
When STORE_DEFAULT_ALL is issued, operating memory should not be written to during the save.