SLVSCQ9E November 2014 – March 2022 TPS65400
PRODUCTION DATA
The USER_DATA_BYTE_01 command contains 7 bits, USER_DATA_BITS_01, for reading and writing user-defined data. Upon issuing STORE_DEFAULT_ALL, contents of this command are saved to the default store in data flash.
The most significant bit, STORED, is a read-only bit that indicates whether the user has written to the default store through STORE_DEFAULT_ALL. This indicator bit cannot be cleared.
BITS | NAME | READ / WRITE | DEFAULT VALUE |
---|---|---|---|
7 | STORED | R | 0 |
6:0 | USER_DATA_BYTE_01 | R/W | 0000000 |
This command has no PAGE support.