SWCS049S June 2010 – August 2018 TPS65911
PRODUCTION DATA.
The power resources provided by the TPS65911 device include inductor based switched mode power supplies (SMPSs) and linear low-dropout voltage regulators (LDOs). These supply resources provide the required power to the external processor cores and external components, and to modules embedded in the TPS65911 device.
Two of the integrated SMPSs and the external FET SMPS have voltage scaling capability. These SMPSs provide independent core voltage domains to the host processor. When changing the output voltage, VDD1 and VDD2 reach the new value through successive steps of 2.5 to 12.5 mV. The size of the voltage step is selected by the TSTEP bit. VDDCtrl has a target slew rate of 100 mV/20 µs. New output values are reached in successive smaller steps of N × LSB, LSB = 12.5 mV, N = 1 to 4. A suitable combination of steps is calculated internally based on current and new target value for output voltage.
The VIO SMPS provides supply voltage for the host processor I/Os.
Table 6-1 lists the power sources provided by the TPS65911 device.