8.4.1.5 FRS (Fast Role Swap) State
In the FRS state, EN1 = 1, EN0 = 1. The FRS state is a transitional state, that transitions automatically from the SNK state to the SRC 3-A state upon successful completion of the fast role swap sequence:
- PPHV power path is automatically disabled
- PPHV overtemperature, VBUS overvoltage (if OVP terminal not grounded) protections are disabled
- VIN and PP5V undervoltage lockout are enabled
- PP5V power path is automatically enabled along with its overvoltage, overtemperature and RCP protection circuits upon successfully completing the fast role swap sequence.
The following transitions are possible from the FRS state:
- SRC 3-A state. This transition is automatic upon successful completion of the fast role swap sequence.
- DISABLED state if:
- (EN1 = 0) or (EN0 = 0). This may allow for exiting a FRS sequence depending on the current status of the FRS sequence.
- SRC FAULT state if:
- PP5V UVLO, PP5V OVP event detected -or-
- PP5V current limit and PP5V TSD events detected