SLVSEW8B August 2019 – December 2019 TPS66020 , TPS66021
PRODUCTION DATA.
When the PP5V power path is enabled, the RCP circuitry monitors the voltage across the path. If the RCP monitor detects VVBUS - VPP5V ≥ VRCP_THRES_PP5V, the PP5V path will be disabled preventing additional current flow from VBUS to PP5V. The power path will be completely disabled and remain disabled as long as the RCP condition persists. After the RCP event, the PP5V path will automatically re-enable. FLT is asserted when a reverse current protection event occurs on the PP5V path.