SBVS337A April 2018 – December 2018 TPS746
PRODUCTION DATA.
As with most LDOs, excessive reverse current can damage this device.
Reverse current flows through the body diode on the pass element instead of the normal conducting channel. At high magnitudes, this current flow degrades the long-term reliability of the device, as a result of one of the following conditions:
Conditions where reverse current can occur are outlined in this section, all of which can exceed the absolute maximum rating of VOUT > VIN + 0.3 V:
If reverse current flow is expected in the application, external protection must be used to protect the device. Figure 49 shows one approach of protecting the device.