SBVS163A June 2011 – May 2015 TPS7A3401
PRODUCTION DATA.
An evaluation module (EVM) is available to assist in the initial circuit performance evaluation using the TPS7A3401. The TPS7A3401EVM-042 evaluation module (and related user's guide) can be requested at the Texas Instruments website through the product folders or purchased directly from the TI eStore.
Computer simulation of circuit performance using SPICE is often useful when analyzing the performance of analog circuits and systems. A SPICE model for the TPS7A3401 is available through the product folder under the Tools & Software tab.
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
PowerPAD, E2E are trademarks of Texas Instruments.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.