The TPS7A4701-EP is a positive voltage (36 V), ultra-low-noise (4 µVRMS) low-dropout linear regulators (LDO) capable of sourcing a 1-A load.
The TPS7A4701-EP output voltage can be configured with a user-programmable PCB layout (up to 20.5 V), or adjustable (up to 34 V) with external feedback resistors.
The TPS7A4701-EP is designed with bipolar technology primarily for high-accuracy, high-precision instrumentation applications where clean voltage rails are critical to maximize system performance. This feature makes the device ideal for powering operational amplifiers, analog-to-digital converters (ADCs), digital-to-analog converters (DACs), and other high-performance analog circuitry in critical applications such as medical, radio frequency (RF), and test-and-measurement.
In addition, the TPS7A4701-EP is ideal for post DC-DC converter regulation. By filtering out the output voltage ripple inherent to DC-DC switching conversions, maximum system performance is ensured in sensitive instrumentation, test-and-measurement, audio, and RF applications.
PART NUMBER | PACKAGE | BODY SIZE (NOM) |
---|---|---|
TPS7A4701-EP | VQFN (20) | 5.00 mm × 5.00 mm |
DATE | REVISION | NOTES |
---|---|---|
February 2017 | * | Initial release. |
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
0P1V | 12 | I | When connected to GND, this pin adds 0.1 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
0P2V | 11 | I | When connected to GND, this pin adds 0.2 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
0P4V | 10 | I | When connected to GND, this pin adds 0.4 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
0P8V | 9 | I | When connected to GND, this pin adds 0.8 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
1P6V | 8 | I | When connected to GND, this pin adds 1.6 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
3P2V | 6 | I | When connected to GND, this pin adds 3.2 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
6P4V1 | 5 | I | When connected to GND, this pin adds 6.4 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
6P4V2 | 4 | I | When connected to GND, this pin adds 6.4 V to the nominal output voltage of the regulator. |
Do not connect any voltage other than GND to this pin. If not used, leave this pin floating. | |||
EN | 13 | I | Enable pin. The device is enabled when the voltage on this pin exceeds the maximum enable voltage, VEN(HI). If enable is not required, tie EN to IN. |
GND | 7 | — | Ground. |
IN | 15, 16 | I | Input supply. A capacitor greater than or equal to 1 µF must be tied from this pin to ground to assure stability. A 10-µF capacitor is recommended to be connected from IN to GND (as close to the device as possible) to reduce circuit sensitivity to printed circuit board (PCB) layout, especially when long input traces or high source impedances are encountered. |
NC | 2, 17-19 | — | This pin can be left open or tied to any voltage between GND and IN. |
NR | 14 | — | Noise reduction pin. When a capacitor is connected from this pin to GND, RMS noise can be reduced to very low levels. A capacitor greater than or equal to 10 nF must be tied from this pin to ground to assure stability. A 1-µF capacitor is recommended to be connected from NR to GND (as close to the device as possible) to maximize ac performance and minimize noise. |
OUT | 1, 20 | O | Regulator output. A capacitor greater than or equal to 10 µF must be tied from this pin to ground to assure stability. A 47-µF ceramic output capacitor is highly recommended to be connected from OUT to GND (as close to the device as possible) to maximize ac performance. |
SENSE/FB | 3 | I | Control-loop error amplifier input. |
This is the SENSE pin if the device output voltage is programmed using ANY-OUT (no external feedback resistors). This pin must be connected to OUT. Connect this pin to the point of load to maximize accuracy. | |||
This is the FB pin if the device output voltage is set using external resistors. See the Adjustable Operation section for more details. | |||
SENSE | 3 | I | This is the SENSE pin of the device and must be connected to OUT. Connect this pin to the point of load to maximize accuracy. |
Thermal Pad | — | Connect the thermal pad to a large-area ground plane. The thermal pad is internally connected to GND. |
MIN | MAX | UNIT | ||||
---|---|---|---|---|---|---|
Voltage(2) | IN pin to GND pin | –0.4 | 36 | V | ||
EN pin to GND pin | –0.4 | 36 | V | |||
EN pin to IN pin | –36 | 0.4 | V | |||
OUT pin to GND pin | –0.4 | 36 | V | |||
NR pin to GND pin | –0.4 | 36 | V | |||
SENSE/FB pin to GND pin | –0.4 | 36 | V | |||
0P1V pin to GND pin | –0.4 | 36 | V | |||
0P2V pin to GND pin | –0.4 | 36 | V | |||
0P4V pin to GND pin | –0.4 | 36 | V | |||
0P8V pin to GND pin | –0.4 | 36 | V | |||
1P6V pin to GND pin | –0.4 | 36 | V | |||
3P2V pin to GND pin | –0.4 | 36 | V | |||
6P4V1 pin to GND pin | –0.4 | 36 | V | |||
6P4V2 pin to GND pin | –0.4 | 36 | V | |||
Current | Peak output | Internally limited | ||||
TJ | Operating virtual junction | –55 | 150 | °C | ||
Tstg | Storage temperature | –65 | 150 | °C |
MIN | MAX | UNIT | ||||
---|---|---|---|---|---|---|
V(ESD) | Electrostatic discharge | Human-body model (HBM), per ANSI/ESDA/JEDEC JS-001, all pins(1) | –2500 | 2500 | V | |
Charged-device model (CDM), per JEDEC specification JESD22-C101, all pins(2) | –500 | 500 |
MIN | NOM | MAX | UNIT | ||
---|---|---|---|---|---|
VI | 3.0 | 35 | V | ||
VO | 1.4 | 34 | V | ||
VEN | 0 | VIN | V | ||
IO | 0 | 1 | A |
THERMAL METRIC(1) | TPS7A4701-EP | UNIT | |
---|---|---|---|
RGW | |||
20 PINS | |||
RθJA | Junction-to-ambient thermal resistance | 32.5 | °C/W |
RθJC(top) | Junction-to-case (top) thermal resistance | 27 | °C/W |
RθJB | Junction-to-board thermal resistance | 11.9 | °C/W |
ψJT | Junction-to-top characterization parameter | 0.3 | °C/W |
ψJB | Junction-to-board characterization parameter | 11.9 | °C/W |
RθJC(bot) | Junction-to-case (bottom) thermal resistance | 1.7 | °C/W |
PARAMETER | TEST CONDITIONS | MIN | TYP | MAX | UNIT | |||
---|---|---|---|---|---|---|---|---|
VI | Input voltage range | 3 | 35 | V | ||||
VUVLO | Under-voltage lockout threshold | VI rising | 2.67 | V | ||||
VI falling | 2.5 | |||||||
V(REF) | Reference voltage | V(REF) = V(FB) | 1.4 | V | ||||
VUVLO(HYS) | Under-voltage lockout hysteresis | 177 | mV | |||||
VNR | Noise reduction pin voltage | Using ANY-OUT option | VOUT | V | ||||
Using adjustable option | 1.4 | |||||||
VO | Output voltage range | VI ≥ VO(nom) + 1 V or 3 V (whichever is greater), COUT = 20 µF |
Using ANY-OUT option | 1.4 | 20.5 | V | ||
Using adjustable option | 1.4 | 34 | ||||||
Nominal accuracy | TJ = 25°C, COUT = 20 µF | –1 | 1 | %VO | ||||
Overall accuracy | VO(nom) + 1 V ≤ VI ≤ 35 V, 0 mA ≤ IO ≤ 1 A, COUT = 20 µF |
–3.5 | 3.5 | |||||
ΔVO(ΔVI) | Line regulation | VO(nom) + 1 V ≤ VI ≤ 35 V | 0.092 | %VO | ||||
ΔVO(ΔIO) | Load regulation | 0 mA ≤ IO ≤ 1 A | 0.3 | %VO | ||||
V(DO) | Dropout voltage | VI = 95% VO(nom), IO = 0.5 A | 216 | mV | ||||
VI = 95% VO(nom), IO = 1 A | 307 | 450 | ||||||
I(CL) | Current limit | VO = 90% VO(nom) | 1 | 1.26 | A | |||
I(GND) | Ground pin current | IO = 0 mA | 0.58 | 1 | mA | |||
IO = 1 A | 6.1 | |||||||
I(EN) | Enable pin current | VEN = VI | 0.78 | 2 | µA | |||
VI = VEN = 35 V | 0.81 | 2 | ||||||
I(SHDN) | Shutdown supply current | VEN = 0.4 V | 2.55 | 8 | µA | |||
VEN = 0.4 V, VI = 35 V | 3.04 | 60 | ||||||
V+EN(HI) | Enable high-level voltage | 2 | VI | V | ||||
V+EN(LO) | Enable low-level voltage | 0 | 0.4 | V | ||||
I(FB) | Feedback pin current | 350 | nA | |||||
PSRR | Power-supply rejection ratio | VI = 16 V, VO(nom) = 15 V, COUT = 50 µF, IO = 500 mA, CNR = 1 µF, f = 1 kHz |
78 | dB | ||||
Vn | Output noise voltage | VI = 3 V, VO(nom) = 1.4 V, COUT = 50 µF, CNR = 1 µF, BW = 10 Hz to 100 kHz |
4.17 | µVRMS | ||||
VIN = 6 V, VO(nom) = 5 V, COUT = 50 µF, CNR = 1 µF, BW = 10 Hz to 100 kHz |
4.67 | |||||||
Tsd | Thermal shutdown temperature | Shutdown, temperature increasing | 170 | °C | ||||
Reset, temperature decreasing | 150 | |||||||
TJ | Operating junction temperature | –55 | 125 | °C |
IOUT = 500 mA | COUT = 50 µF | CNR = 1 µF |
BWRMSNOISE (10 Hz, 100 kHz) |
IOUT = 1 A | COUT = 50 µF | VIN = 3 V |
VOUT = 1.4 V |
CNR = 1 µF | COUT = 50 µF | VIN = 3 V |
VOUT = 1.4 V |
VOUT = 3.3 V | CNR = 1 µF | COUT = 50 µF |
IOUT = 500 mA |
CNR = 1 µF | COUT = 50 µF | IOUT = 500 mA |
VIN = 5 V | VOUT = 3.3 V | IOUT = 10 mA to 845 mA |
Startup Time = 65 ms | VIN = 6 V | VOUT = 5 V |
IOUT = 500 mA | CIN = 10 µF | COUT = 50 µF |
IOUT = 0 µA |
VOUT = 90% VOUT(NOM) |
IOUT = 0.5 A | COUT = 50 µF | VIN = 3 V |
VOUT = 1.4 V |
VOUT = 3.3 V | CNR = 1 µF | COUT = 50 µF |
IOUT = 50 mA |
VOUT = 3.3 V | CNR = 1 µF | COUT = 50 µF |
IOUT = 1 A |
CNR = 1 µF | COUT = 50 µF | IOUT = 1000 mA |
VIN = 5 V to 15 V | VOUT = 3.3 V | IOUT = 845 mA |
VOUT = 4.7 V | COUT = 10 µF | CNR = 1 µF |
BWRMSNOISE (10 Hz, 100 kHz) |
The TPS7A4701-EP is a positive voltage (36 V), ultra-low-noise (4 µVRMS) LDOs capable of sourcing a 1-A load. The TPS7A4701-EP is designed with bipolar technology primarily for high-accuracy, high-precision instrumentation applications where clean voltage rails are critical to maximize system performance. This feature makes the device ideal for powering operational amplifiers, analog-to-digital converters (ADCs), digital-to-analog converters (DACs), and other high-performance analog circuitry.
The internal current limit circuit is used to protect the LDO against high-load current faults or shorting events. The LDO is not designed to operate at a steady-state current limit. During a current-limit event, the LDO sources constant current. Therefore, the output voltage falls while load impedance decreases. Note also that when a current limit occurs while the resulting output voltage is low, excessive power is dissipated across the LDO, which results in a thermal shutdown of the output.
The TPS7A4701-EP only turns on when both EN and UVLO are above the respective voltage thresholds. The UVLO circuit monitors input voltage (VI) to prevent device turnon before VI rises above the lockout voltage. The UVLO circuit also causes a shutdown when VI falls below lockout. The EN signal allows independent logic-level turnon and shutdown of the LDO when the input voltage is present. EN can be connected directly to VI if independent turnon is not needed.
Soft-start refers to the ramp-up characteristic of the output voltage during LDO turnon after EN and UVLO have achieved threshold voltage. The noise reduction capacitor serves a dual purpose of both governing output noise reduction and programming the soft-start ramp during turnon.
Inrush current is defined as the current through the LDO from IN to OUT during the time of the turnon ramp up. Inrush current then consists primarily of the sum of load and charge current to the output capacitor. Inrush current can be estimated by Equation 1:
where
The TPS7A4701-EP has the following functional modes:
TPS7A4701-EP can be used in ANY-OUT mode. For ANY-OUT operation, the device does not use external resistors to set the output voltage, but uses device pins 4, 5, 6, 8, 9, 10, 11, and 12 to program the regulated output voltage. Each pin is either connected to ground (active) or is left open (floating). The ANY-OUT programming is set by Equation 2 as the sum of the internal reference voltage (V(REF) = 1.4 V) plus the accumulated sum of the respective voltages assigned to each active pin; that is, 100 mV (pin 12), 200 mV (pin 11), 400 mV (pin 10), 800 mV (pin 9), 1.6 V (pin 8), 3.2 V (pin 6), 6.4 V (pin 5), or 6.4 V (pin 4). Table 1 summarizes these voltage values associated with each active pin setting for reference. By leaving all program pins open, or floating, the output is thereby programmed to the minimum possible output voltage equal to V(REF).
ANY-OUT PROGRAM PINS (Active Low) | ADDITIVE OUTPUT VOLTAGE LEVEL |
---|---|
Pin 4 (6P4V2) | 6.4 V |
Pin 5 (6P4V1) | 6.4 V |
Pin 6 (3P2) | 3.2 V |
Pin 8 (1P6) | 1.6 V |
Pin 9 (0P8) | 800 mV |
Pin 10 (0P4) | 400 mV |
Pin 11 (0P2) | 200 mV |
Pin 12 (0P1) | 100 mV |
Table 2 shows a list of the most common output voltages and the corresponding pin settings. The voltage setting pins have a binary weight; therefore, the output voltage can be programmed to any value from 1.4 V to 20.5 V in 100-mV steps.
VO (V) | PIN NAMES AND VOLTAGE PER PIN | |||||||
---|---|---|---|---|---|---|---|---|
0P1V 100 mV |
0P2V 200 mV |
0P4V 400 mV |
0P8V 800 mV |
1P6V 1.6 V |
3P2V 3.2 V |
6P4V1 6.4 V |
6P4V2 6.4 V |
|
1.4 | Open | Open | Open | Open | Open | Open | Open | Open |
1.5 | GND | Open | Open | Open | Open | Open | Open | Open |
1.8 | Open | Open | GND | Open | Open | Open | Open | Open |
2.5 | GND | GND | Open | GND | Open | Open | Open | Open |
3 | Open | Open | Open | Open | GND | Open | Open | Open |
3.3 | GND | GND | Open | Open | GND | Open | Open | Open |
4.5 | GND | GND | GND | GND | GND | Open | Open | Open |
5 | Open | Open | GND | Open | Open | GND | Open | Open |
10 | Open | GND | GND | Open | GND | Open | GND | Open |
12 | Open | GND | Open | GND | Open | GND | GND | Open |
15 | Open | Open | Open | GND | Open | Open | GND | GND |
18 | Open | GND | GND | Open | Open | GND | GND | GND |
20.5 | GND | GND | GND | GND | GND | GND | GND | GND |
The TPS7A4701-EP has an output voltage range of 1.4 V to 34 V. For adjustable operation, set the nominal output voltage of the device using two external resistors, as shown in Figure 23.
R1 and R2 can be calculated for any output voltage within the operational range. The current through feedback resistor R2 must be at least 5 µA to ensure stability. Additionally, the current into the FB pin (I(FB), typically 350 nA) creates an additional output voltage offset that depends on the resistance of R1. For high-accuracy applications, select R2 such that the current through R2 is at least 35 µA to minimize any effects of I(FB) variation on the output voltage; 10 kΩ is recommended. R1 can be calculated using Equation 3.
Use 0.1% tolerance resistors to minimize the effects of resistor inaccuracy on the output voltage.
Table 3 shows the resistor combinations to achieve some standard rail voltages with commercially-available 1% tolerance resistors. The resulting output voltages yield a nominal error of < 0.5%.
VOUT | R1, Calculated | R1, Closest 1% Value | R2 |
---|---|---|---|
1.4 V | 0 Ω | 0 Ω | ∞ |
1.8 V | 2.782 kΩ | 2.8 kΩ | 9.76 kΩ |
3.3 V | 13.213 kΩ | 13.3 kΩ | 9.76 kΩ |
5 V | 25.650 kΩ | 25.5 kΩ | 10 kΩ |
12 V | 77.032 kΩ | 76.8 kΩ | 10.2 kΩ |
15 V | 101.733 kΩ | 102 kΩ | 10.5 kΩ |
18 V | 118.276 kΩ | 118 kΩ | 10 kΩ |
24 V | 164.238 kΩ | 165 kΩ | 10.2 kΩ |
To achieve higher nominal accuracy, two resistors can be used in the place of R1. Select the two resistor values such that the sum results in a value as close as possible to the calculated R1 value.
There are several alternative ways to set the output voltage. The program pins can be pulled low using external general-purpose input/output pins (GPIOs), or can be hardwired by the given layout of the printed circuit board (PCB) to set the ANY-OUT voltage. The TPS7A4701 evaluation module (EVM), available for purchase from the TI eStore, allows the output voltage to be programmed using jumpers.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS7A740x is a high-voltage, low-noise, 1-A LDO. Low-noise performance makes this LDO ideal for providing rail voltages to noise-sensitive loads, such as PLLs, oscillators, and high-speed ADCs.
Output voltage is set by grounding the appropriate control pins, as shown in Figure 24. When grounded, all control pins add a specific voltage on top of the internal reference voltage (V(REF) = 1.4 V). For example, when grounding pins 0P1V, 0P2V, and 1P6V, the voltage values 0.1 V, 0.2 V, and 1.6 V are added to the 1.4-V internal reference voltage for VO(nom) equal to 3.3 V, as described in the Programming section.
PARAMETER | DESIGN REQUIREMENT |
---|---|
Input Voltage | 5 V, ±10% |
Output Voltage | 3.3 V, ±3% |
Output Current | 500 mA |
Peak-to-Peak Noise, 10 Hz to 100 kHz | 50 µVp-p |
These LDOs are designed to be stable using low equivalent series resistance (ESR), ceramic capacitors at the input, output, and at the noise reduction pin (NR, pin 14). Multilayer ceramic capacitors have become the industry standard for these types of applications and are recommended here, but must be used with good judgment. Ceramic capacitors that employ X7R-, X5R-, and COG-rated dielectric materials provide relatively good capacitive stability across temperature, but the use of Y5V-rated capacitors is discouraged precisely because the capacitance varies so widely. In all cases, ceramic capacitance varies a great deal with operating voltage and the design engineer must be aware of these characteristics. It is recommended to apply a 50% derating of the nominal capacitance in the design.
Attention must be given to the input capacitance to minimize transient input droop during load current steps because the TPS7A4701-EP has a very fast load transient response. Large input capacitors are necessary for good transient load response, and have no detrimental influence on the stability of the device. Note, however, that using large ceramic input capacitances can also cause unwanted ringing at the output if the input capacitor, in combination with the wire lead inductance, creates a high-Q peaking effect during transients. For example, a 5-nH lead inductance and a 10-µF input capacitor form an LC filter with a resonance frequency of 712 kHz at the edge of the control loop bandwidth. Short, well-designed interconnect leads to the up-stream supply minimize this effect without adding damping. Damping of unwanted ringing can be accomplished by using a tantalum capacitor, with a few hundred milliohms of ESR, in parallel with the ceramic input capacitor.
The TPS7A4701-EP is designed and characterized for operation with ceramic capacitors of 10 µF or greater at the input and output. Optimal noise performance is characterized using a total output capacitor value of 50 µF. Note especially that input and output capacitances must be located as near as practical to the respective input and output pins.
The noise reduction capacitor, connected to the NR pin of the LDO, forms an RC filter for filtering out noise that might ordinarily be amplified by the control loop and appear on the output voltage. Larger capacitances, up to 1 µF, affect noise reduction at lower frequencies while also tending to further reduce noise at higher frequencies. Note that CNR also serves a secondary purpose in programming the turnon rise time of the output voltage and thereby controls the turnon surge current.
Generally speaking, the dropout voltage often refers to the voltage difference between the input and output voltage (V(DO) = VI – VO). However, in the Electrical Characteristics V(DO) is defined as the VI – VO voltage at the rated current (I(RATED)), where the main current pass-FET is fully on in the Ohmic region of operation and is characterized by the classic RDS(on) of the FET. V(DO) indirectly specifies a minimum input voltage above the nominal programmed output voltage at which the output voltage is expected to remain within its accuracy boundary. If the input falls below this V(DO) limit (VI < VO + V(DO)), then the output voltage decreases in order to follow the input voltage.
Dropout voltage is always determined by the RDS(on) of the main pass-FET. Therefore, if the LDO operates below the rated current, the V(DO) is directly proportional to the output current and can be reduced by the same factor. The RDS(on) for the TPS7A4701-EP can be calculated using Equation 4:
The output voltage accuracy specifies minimum and maximum output voltage error, relative to the expected nominal output voltage stated as a percent. This accuracy error typically includes the errors introduced by the internal reference and the load and line regulation across the full range of rated load and line operating conditions over temperature, unless otherwise specified by the Electrical Characteristics. Output voltage accuracy also accounts for all variations between manufacturing lots.
The startup time for the TPS7A4701-EP depends on the output voltage and the capacitance of the CNR capacitor. Equation 5 calculates the startup time for a typical device.
where
AC performance of the LDO is typically understood to include power-supply rejection ratio, load step transient response, and output noise. These metrics are primarily a function of open-loop gain and bandwidth, phase margin, and reference noise.
PSRR is a measure of how well the LDO control loop rejects ripple noise from the input source to make the DC output voltage as noise-free as possible across the frequency spectrum (usually 10 Hz to 10 MHz). Equation 6 gives the PSRR calculation as a function of frequency where input noise voltage [VS(IN)(f)] and output noise voltage [VS(OUT)(f)] are understood to be purely ac signals.
Noise that couples from the input to the internal reference voltage for the control loop is also a primary contributor to reduced PSRR magnitude and bandwidth. This reference noise is greatly filtered by the noise reduction capacitor at the NR pin of the LDO in combination with an internal filter resistor (RSS) for optimal PSRR.
The LDO is often employed not only as a DC-DC regulator, but also to provide exceptionally clean power-supply voltages that are free of noise and ripple to power-sensitive system components. This usage is especially true for the TPS7A4701-EP.
The load step transient response is the output voltage response by the LDO to a step change in load current whereby output voltage regulation is maintained. The worst-case response is characterized for a load step of
10 mA to 1 A (at 1 A per microsecond) and shows a classic, critically-damped response of a very stable system. The voltage response shows a small dip in the output voltage when charge is initially depleted from the output capacitor and then the output recovers as the control loop adjusts itself. The depth of the charge depletion immediately after the load step is directly proportional to the amount of output capacitance. However, to some extent, the speed of recovery is inversely proportional to that same output capacitance. In other words, larger output capacitances act to decrease any voltage dip or peak occurring during a load step but also decrease the control-loop bandwidth, thereby slowing response.
The worst-case, off-loading step characterization occurs when the current step transitions from 1 A to 0 mA. Initially, the LDO loop cannot respond fast enough to prevent a small increase in output voltage charge on the output capacitor. Because the LDO cannot sink charge current, the control loop must turn off the main pass-FET to wait for the charge to deplete, thus giving the off-load step its typical monotonic decay (which appears triangular in shape).
The TPS7A4701-EP is designed, in particular, for system applications where minimizing noise on the power-supply rail is critical to system performance. This scenario is the case for phase-locked loop (PLL)-based clocking circuits for instance, where minimum phase noise is all important, or in-test and measurement systems where even small power-supply noise fluctuations can distort instantaneous measurement accuracy. Because the TPS7A4701-EP is also designed for higher voltage industrial applications, the noise characteristic is well designed to minimize any increase as a function of the output voltage.
LDO noise is defined as the internally-generated intrinsic noise created by the semiconductor circuits alone. This noise is the sum of various types of noise (such as shot noise associated with current-through-pin junctions, thermal noise caused by thermal agitation of charge carriers, flicker or 1/f noise that is a property of resistors and dominates at lower frequencies as a function of 1/f, burst noise, and avalanche noise).
To calculate the LDO RMS output noise, a spectrum analyzer must first measure the spectral noise across the bandwidth of choice (typically 10 Hz to 100 kHz in units of µV/√Hz). The RMS noise is then calculated in the usual manner as the integrated square root of the squared spectral noise over the band, then averaged by the bandwidth.
The device is designed to operate from an input voltage supply range of 3 V to 35 V. If the input supply is noisy, additional input capacitors with low ESR can help improve the output noise performance.
Power dissipation must be considered in the PCB design. In order to minimize risk of device operation above 125°C, use as much copper area as available for thermal dissipation. Do not locate other power-dissipating devices near the LDO.
Power dissipation in the regulator depends on the input to output voltage difference and load conditions. PD can be calculated using Equation 7:
It is important to note that power dissipation can be minimized, and thus greater efficiency achieved, by proper selection of the system voltage rails. Proper selection allows the minimum input voltage necessary for output regulation to be obtained.
The primary heat conduction path for the QFN (RGW) package is through the thermal pad to the PCB. The thermal pad must be soldered to a copper pad area under the device. Thermal vias are recommended to improve the thermal conduction to other layers of the PCB.
The maximum power dissipation determines the maximum allowable junction temperature (TJ) for the device. Power dissipation and junction temperature are most often related by the junction-to-ambient thermal resistance (θJA) of the combined PCB and device package and the temperature of the ambient air (TA), according to Equation 8.
Unfortunately, this thermal resistance (θJA) depends primarily on the heat-spreading capability built into the particular PCB design, and therefore varies according to the total copper area, copper weight, and location of the spreading planes. The θJA recorded in the Thermal Information table is determined by the JEDEC standard, PCB, and copper-spreading area and is to be used only as a relative measure of package thermal performance. Note that for a well-designed thermal layout, θJA is actually the sum of the QFN package junction-to-case (bottom) thermal resistance (θJCbot) plus the thermal resistance contribution by the PCB copper. By knowing θJCbot, the minimum amount of appropriate heat sinking can be used to estimate θJA with Figure 27. θJCbot can be found in the Thermal Information table.
NOINDENT:
NOTE: θJA value at a board size of 9-in2 (that is, 3-in × 3-in) is a JEDEC standard.For best overall performance, all circuit components are recommended to be located on the same side of the circuit board and as near as practical to the respective LDO pin connections. Ground return connections to the input and output capacitor, and to the LDO ground pin, must also be as close to each other as possible and connected by a wide, component-side, copper surface. The use of vias and long traces to create LDO circuit connections is strongly discouraged and negatively affects system performance. This grounding and layout scheme minimizes inductive parasitics and thereby reduces load-current transients, minimizes noise, and increases circuit stability.
A ground reference plane is also recommended. This reference plane serves to assure accuracy of the output voltage, shield noise, and behaves similar to a thermal plane to spread (or sink) heat from the LDO device when connected to the PowerPAD™. In most applications, this ground plane is necessary to meet thermal requirements.
Use the TPS7A4701 evaluation module (EVM), available for purchase from the TI eStore, as a reference for layout and application design.
The TPS7A4701-EP contains a thermal shutdown protection circuit to turn off the output current when excessive heat is dissipated in the LDO. Thermal shutdown occurs when the thermal junction temperature (TJ) of the main pass-FET exceeds 170°C (typical). Thermal shutdown hysteresis assures that the LDO again resets (turns on) when the temperature falls to 150°C (typical). Because the TPS7A4701-EP is capable of supporting high input voltages, a great deal of power can be expected to be dissipated across the device at low output voltages, which causes a thermal shutdown. The thermal time-constant of the semiconductor die is fairly short, and thus the output oscillates on and off at a high rate when thermal shutdown is reached until power dissipation is reduced.
For reliable operation, the junction temperature must be limited to a maximum of 125°C. To estimate the thermal margin in a given layout, increase the ambient temperature until the thermal protection shutdown is triggered using worst-case load and highest input voltage conditions. For good reliability, thermal shutdown must be designed to occur at least 45°C above the maximum expected ambient temperature condition for the application. This configuration produces a worst-case junction temperature of 125°C at the highest expected ambient temperature and worst-case load.
The internal protection circuitry of the TPS7A4701-EP is designed to protect against thermal overload conditions. The circuitry is not intended to replace proper heat sinking. Continuously running the TPS7A4701-EP into thermal shutdown degrades device reliability.
JEDEC standards now recommend the use of PSI thermal metrics to estimate the junction temperatures of the LDO while in-circuit on a typical PCB board application. These metrics are not strictly speaking thermal resistances, but rather offer practical and relative means of estimating junction temperatures. These PSI metrics are determined to be significantly independent of copper-spreading area. The key thermal metrics (ΨJT and ΨJB) are given in the Thermal Information table and are used in accordance with Equation 9.
where