SBVS289A August 2017 – September 2017 TPS7A88-Q1
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
An evaluation module (EVM) is available to assist in the initial circuit performance evaluation using the TPS7A88-Q1. The summary information for this fixture is listed in Table 10.
NAME | PART NUMBER |
---|---|
TPS7A88- Low-Dropout Voltage Regulator Evaluation Module | TPS7A88EVM-776 |
The EVM can be requested at the Texas Instruments website (www.ti.com) through the TPS7A88-Q1 product folder.
Computer simulation of circuit performance using spice is often useful when analyzing the performance of analog circuits and systems. A spice model for the TPS7A88-Q1 is available through the TPS7A88-Q1 product folder under simulation models.
PRODUCT | DESCRIPTION |
---|---|
TPS7A88xxQYYYZ -Q1 | YYY is the package designator. XX represents the output voltage. 01 is the adjustable output version. Z is the package quantity. |
TPS3780 Data Sheet (SBVS250)
TPS7A88 Evaluation Module (SBVU027)
Pros and Cons of Using a Feed-Forward Capacitor with a Low Dropout Regulator (SBVA042)
How to Measure LDO Noise (SLYY076)
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
All other trademarks are the property of their respective owners.
This integrated circuit can be damaged by ESD. Texas Instruments recommends that all integrated circuits be handled with appropriate precautions. Failure to observe proper handling and installation procedures can cause damage.
ESD damage can range from subtle performance degradation to complete device failure. Precision integrated circuits may be more susceptible to damage because very small parametric changes could cause the device not to meet its published specifications.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.