SBVS441 December 2022 TPS7B4255
PRODUCTION DATA
This device is a tracking LDO; thus, the output voltage is determined by the voltage provided to the ADJ/EN pin, provided that VIN is greater than VIH. When the voltage at the ADJ/EN pin exceeds the required voltage to enable the LDO (VIH), the output begins to rise to the voltage on the ADJ/EN pin. The output rises linearly as determined by the load, the output capacitor, and the current limit. When the voltage reaches the level on the ADJ/EN pin, the output voltage remains within 5 mV from the voltage set on the ADJ/EN pin over all specified operating conditions.