SBVS441 December 2022 TPS7B4255
PRODUCTION DATA
The device has an internally fixed undervoltage lockout threshold. Undervoltage lockout activates when the input voltage on VIN drops below the undervoltage lockout (UVLO) level (see the VUVLO(FALLING) parameter in the Section 6.5 table). This activation makes sure the regulator is not latched into an unknown state during a low input supply voltage. If the input voltage has a negative transient that drops below the UVLO threshold and recovers, the regulator shuts down and powers up in the standard power-up sequence when the input voltage recovers to the required level (see the VUVLO(RISING) parameter in the Section 6.5 table).