SNOSDE3C July 2023 – April 2024 TPS7H6003-SP , TPS7H6013-SP , TPS7H6023-SP
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Gate drive devices such as the TPS7H6003-SP have several different components that comprise the power losses. The quiescent power losses PQCcan be determined using Equation 21 :
where:
Leakage current power losses PBG can be calculated using Equation 22 :
where:
There are losses that occur within the driver due to the charging and discharging of the GaN FET gate charge. To determine these, first calculate PGATE as:
This loss is actually distributed amongst the resistances in the gate driver loop, which includes the driver, the gate resistances and the GaN FET. The power dissipated within the TPS7H6003-SP for both turn-on and turn-off can be calculated:
In this instance, the high-side and low-side losses are the same:
Finally, the PGATE losses within the driver can be found:
There is also a component power consumption associated with the operating current of the driver itself, which is specified at no-load and frequency dependent. These can be approximated using the operating current parameters in the Specifications section:
where: