SBVS445A October 2024 – December 2024 TPS7N53
PRODUCTION DATA
Noise can be generally defined as any unwanted signal combining with the desired signal (such as the regulated LDO output) that results in degraded power-supply source quality. Noise can be easily noticed in audio as a hissing or popping sound. Extrinsic and intrinsic are the two basic groups that noise can be categorized into. Noise produced from an external circuit or natural phenomena such as 50 to 60 hertz power-line noise (spikes), along with the harmonics, is an excellent representative of extrinsic noise. Intrinsic noise is produced by components within the device circuitry such as resistors and transistors. For this device, the two dominating sources of intrinsic noise are the error amplifier and the internal reference voltage (VREF). Another term that sometimes combines with extrinsic noise is PSRR, which refers to the ability of the circuit or device to reject or filter out input supply noise and is expressed as a ratio of output voltage noise ripple to input voltage noise ripple.
Optimize the device intrinsic noise and PSRR by carefully selecting:
The device noise performance can be significantly improved by using a larger CNR capacitor to filter out noise coupling from the input into the device VREF reference. This coupling is especially apparent from low frequencies up to the device bandwidth. The low-pass filter formed by CNR and RREF can be designed to target low-frequency noise originating in the input supply. One downside of a larger CNR/SS capacitor is a longer start-up time. The device unity-gain configuration eliminates the noise performance degradation that other LDOs suffer from because of the feedback network. Furthermore, increasing the device load current has little to no effect on the device noise performance.
Further improvement to the device noise at a higher frequency range than the device bandwidth can be achieved by using a larger COUT capacitor. However, a larger COUT increases inrush current and slows down the device transient response.
Increasing the operational headroom between VIN and VOUT has little to no effect on improving noise performance. However, this increase does improve PSRR significantly for frequency ranges up to the device bandwidth. Higher headroom can also improve transient performance of the device as well. Although COUT has little to no affect on improving PSRR at low frequency, COUT can improve PSRR for higher frequencies beyond the device bandwidth. A combination of capacitors, such as 10 μF || 22μF provide and effective combination by lowering ESR and ESL. This behavior is illustrated in Figure 5-3.
Vn (μVRMS), 10-Hz to 100-kHz BW | CNR (µF) | COUT (µF) |
---|---|---|
3.03 | 1 | 22 |
2.2 | 4.7 | 10 |