SLVSHL8 November 2024 TPS923650
PRODUCTION DATA
The maximum LED current is 1A at 2V analog input and the corresponding VREF is 200mV. By using , the sense resistance is calculated as 200mΩ.
Note that the power consumption of the sense resistor is 200mW, requiring enough margin of the resistor's power rating in selection.