SNVSBY8 March 2021 TPS92391
PRODUCTION DATA
The LEDSET resistor missing or invalid is detected if the resistor is not assembled or not valid value as requested during the initialization. The TPS92391 device defaults to 6-channel/200-mA configuration if the LEDSET resistor is missing or invalid. The LEDSET_STATUS fault bit is set in the BOOST_FAULT_STATUS register. The LEDSET resistor missing or invalid fault will not be monitored after initialization, so that the TPS92391 is operating in the configuration determined during initialization even though the LEDSET resistor is missing or invalid after initialization.