SLUSBP5E March 2014 – July 2018 TPS92601-Q1 , TPS92602-Q1
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
The constant output current of the TPS92602y-Q1 device is adjustable by using the external current-shunt resistor. In the application circuit of Figure 16, R5 is the channel 1 current-shunt resistor, and R16 is the channel-2 current shunt resistor. Equation 12 and Equation 13 calculate the resistors that determine maximum output current.