SLVSCK5C September 2014 – January 2020 TPS92638-Q1
PRODUCTION DATA.
Independent linear current regulators control the eight LED output channels. Global external resistors set the current of each channel. The device also features two current levels, intended for stop and tail applications.
The internal current reference, I(REF), has two possible values depending on the state of the STOP input: When STOP is low, REF, the current drawn from the REF pin, controls the output current. When STOP is high, the sum of the currents drawn from the REFHI pin and REF pin controls the output current.
Equations Equation 1 and Equation 2 calculate values for the current-setting resistors:
when STOP = low
when STOP = high
where
Vref is the internal reference voltage
G(I) is the ratio of output current to reference current